Keysight VISA.NET Help
ReadLineListOfByte() Method



Read a comma separated list of bytes from the formatted I/O read buffer and store them into the return array starting at index 0, then read and discard characters up to and including the next newline character.
Syntax
'Declaration
 
Overloads Function ReadLineListOfByte() As Byte()
'Usage
 
Dim instance As IMessageBasedFormattedIO
Dim value() As Byte
 
value = instance.ReadLineListOfByte()
byte[] ReadLineListOfByte()
array<byte>^ ReadLineListOfByte(); 

Return Value

An array of bytes.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025