Keysight VISA.NET Help
ReadLineListOfSingle() Method



Read a comma separated list of single precision reals from the formatted I/O read buffer and store them into the return array starting at index 0, then read and discard characters up to and including the next newline character.
Syntax
'Declaration
 
Overloads Function ReadLineListOfSingle() As Single()
'Usage
 
Dim instance As IMessageBasedFormattedIO
Dim value() As Single
 
value = instance.ReadLineListOfSingle()
float[] ReadLineListOfSingle()
array<float>^ ReadLineListOfSingle(); 

Return Value

An array of single precision reals.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025