Keysight VISA.NET Help
ReadListOfSingle Method



See Using Read Methods for detailed information.
Overload List
OverloadDescription
ReadListOfSingle(Int64)Read a comma separated list of single precision reals from the formatted I/O read buffer and store a maximum of count elements into the return array starting at index 0.  
ReadListOfSingle(Single[],Int64,Int64)Read a comma separated list of single precision reals from the formatted I/O read buffer and store a maximum of count elements into data starting at index.  
Remarks

The ReadListOfSingle method exhibits the same behavior as Scanf("%,g", out result ), which returns result.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025