Keysight VISA.NET Help
Write Method (IMessageBasedFormattedIO)



See Using Write Methods for detailed information.

Overload List
OverloadDescription
Write(Char) Converts the specified character to an ASCII character and appends it to the formatted I/O write buffer.  
Write(String) Converts the specified string to an ASCII string and appends it to the formatted I/O write buffer.  
Write(Int64) Converts the specified signed integer to an ASCII string and appends it to the formatted I/O write buffer.  
Write(UInt64) Converts the specified unsigned integer to an ASCII string and appends it to the formatted I/O write buffer.  
Write(Double) Converts the specified real number to an ASCII string and appends it to the formatted I/O write buffer.  
Remarks

Each Write method exhibits the same behavior as the corresponding call to Printf shown in the following table:

Write Method Equivalent Printf Call
void Write(Char data); Printf("%c", data);
void Write(String data); Printf("%s", data);
void Write(Int64 data); Printf("%@1d", data);
void Write(UInt64 data); Printf("%@1u", data);
void Write(Double data); Printf("%@2f", data);

 

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025