| Ivi.Visa Namespace > IMessageBasedRawIO Interface : ReadString Method |
| Overload | Description |
|---|---|
| ReadString() | Read characters into the return string until an END indicator or termination character is reached. |
| ReadString(Int64) | Read count characters into the return string, or until an END indicator or termination character is reached, whichever comes first. |
| ReadString(Int64,ReadStatus) | Read count characters into the return string, or until an END indicator or termination character is reached, whichever comes first. |
Current with Keysight IO Libraries Suite 18