Keysight VISA.NET Help
INativeVisaSession Interface Methods

For a list of all members of this type, see INativeVisaSession members.

Public Methods
 NameDescription
 MethodDisableEventDisables a client from receiving events of type(s) specified by the eventType argument.  
 MethodDiscardEventsDiscard all pending events of type(s) specified by the eventType argument.  
 MethodDispose (Inherited from System.IDisposable)
 MethodEnableEventEnables a client to receive events of the type specified by the eventType argument using a WaitOnEvent method.  
 MethodGetAttributeBooleanOverloaded.  Retrieve the value of the specified attribute from the underlying VISA C implementation.  
 MethodGetAttributeByteOverloaded.  Retrieve the value of the specified attribute from the underlying VISA C implementation.  
 MethodGetAttributeInt16Overloaded.  Retrieve the value of the specified attribute from the underlying VISA C implementation.  
 MethodGetAttributeInt32Overloaded.  Retrieve the value of the specified attribute from the underlying VISA C implementation.  
 MethodGetAttributeInt64Overloaded.  Retrieve the value of the specified attribute from the underlying VISA C implementation.  
 MethodGetAttributeStringOverloaded.  Retrieve the value of the specified attribute from the underlying VISA C implementation.  
 MethodLockResource Locks the resource for this session with an exclusive lock, with an infinite timeout. (Inherited from Ivi.Visa.IVisaSession)
 MethodSetAttributeBooleanOverloaded.  Set the value of the specified attribute in the underlying VISA C implementation.  
 MethodSetAttributeByteOverloaded.  Set the value of the specified attribute in the underlying VISA C implementation.  
 MethodSetAttributeInt16Overloaded.  Set the value of the specified attribute in the underlying VISA C implementation.  
 MethodSetAttributeInt32Overloaded.  Set the value of the specified attribute in the underlying VISA C implementation.  
 MethodSetAttributeInt64Overloaded.  Set the value of the specified attribute in the underlying VISA C implementation.  
 MethodSetAttributeStringOverloaded.  Set the value of the specified attribute in the underlying VISA C implementation.  
 MethodUnlockResource Unlock the resource. (Inherited from Ivi.Visa.IVisaSession)
 MethodWaitOnEventOverloaded. Wait for events of type(s) specified by the EventType argument.  
Top
See Also

Reference

INativeVisaSession Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025