| Ivi.Visa Namespace > IOTimeoutException Class : IOTimeoutException Constructor |
| Overload | Description |
|---|---|
| IOTimeoutException Constructor(Int64,Byte[]) | Initializes a new instance of the IOTimeoutException class with the specified value for the actual number of elements read or written. |
| IOTimeoutException Constructor(Int64,Byte[],String) | Initializes a new instance of the IOTimeoutException class with the specified value for the actual number of elements read or written and the specified message. |
| IOTimeoutException Constructor(Int64,Byte[],String,Exception) | Initializes a new instance of the IOTimeoutException class with the specified value for the actual number of elements read or written, the specified message, and a reference to the inner exception that is the cause of this exception. |
| IOTimeoutException Constructor(SerializationInfo,StreamingContext) | Initializes a new instance of the IOTimeoutException class with serialized data. |
Current with Keysight IO Libraries Suite 18