Keysight VISA.NET Help
IPxiBackplaneSession Interface Methods

For a list of all members of this type, see IPxiBackplaneSession members.

Public Methods
 NameDescription
 MethodDisableEventDisables a client from receiving events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDiscardEventsDiscard all pending events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDispose (Inherited from System.IDisposable)
 MethodEnableEventEnables a client to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Ivi.Visa.IVisaSession)
 MethodLockResource Locks the resource for this session with an exclusive lock, with an infinite timeout. (Inherited from Ivi.Visa.IVisaSession)
 MethodMapTriggerOverloaded.  Map the specified source trigger line to the specified destination trigger line.  
 MethodReserveTrigger Reserve a single trigger line that the caller can then map and/or assert.  
 MethodReserveTriggersReserve multiple trigger lines that the caller can then map and/or assert. This method will succeed only if it can reserve all of the bus/line pairs. If any of the bus/line pairs cannot be reserved, this method will not reserve any of them. Note that the buses and lines arrays are parallel: the lengths must be the same, and buses[n] corresponds to lines[n].  
 MethodUnlockResource Unlock the resource. (Inherited from Ivi.Visa.IVisaSession)
 MethodUnmapTriggerOverloaded.  Unmap all destination trigger lines to which the specified source trigger line is currently connected.  
 MethodUnreserveTrigger Unreserve a single trigger line that the caller previously reserved.  
 MethodWaitOnEventWait for events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
Top
See Also

Reference

IPxiBackplaneSession Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025