| Ivi.Visa Namespace : IPxiMemorySession Interface |
For a list of all members of this type, see IPxiMemorySession members.
| Name | Description | |
|---|---|---|
![]() | DisableEvent | Disables a client from receiving events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession) |
![]() | DiscardEvents | Discard all pending events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession) |
![]() | Dispose | (Inherited from System.IDisposable) |
![]() | EnableEvent | Enables a client to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Ivi.Visa.IVisaSession) |
![]() | In16 | Read in a 16-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | In32 | Read in a 32-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | In64 | Read in a 64-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | In8 | Read in an 8-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | LockResource | Locks the resource for this session with an exclusive lock, with an infinite timeout. (Inherited from Ivi.Visa.IVisaSession) |
![]() | MapAddress | Map the specified memory space into this process’s address space. (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MemoryAllocate | Overloaded. Allocate memory from the device’s memory region. |
![]() | MemoryFree | Free previously allocated memory. |
![]() | MoveIn16 | Move a 16-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveIn32 | Move a 32-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveIn64 | Move a 64-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveIn8 | Move an 8-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveOut16 | Moves an 16-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveOut32 | Moves an 32-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveOut64 | Moves an 64-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | MoveOut8 | Moves an 8-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | Out16 | Write a 16-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | Out32 | Write a 32-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | Out64 | Write a 64-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | Out8 | Write an 8-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession) |
![]() | UnlockResource | Unlock the resource. (Inherited from Ivi.Visa.IVisaSession) |
![]() | WaitOnEvent | Wait for events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession) |