Keysight VISA.NET Help
IRegisterBasedSession Interface Methods

For a list of all members of this type, see IRegisterBasedSession members.

Public Methods
 NameDescription
 MethodDisableEventDisables a client from receiving events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDiscardEventsDiscard all pending events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDispose (Inherited from System.IDisposable)
 MethodEnableEventEnables a client to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Ivi.Visa.IVisaSession)
 MethodIn16 Read in a 16-bit value from the specified memory space (assigned memory base + offset).  
 MethodIn32 Read in a 32-bit value from the specified memory space (assigned memory base + offset).  
 MethodIn64 Read in a 64-bit value from the specified memory space (assigned memory base + offset).  
 MethodIn8 Read in an 8-bit value from the specified memory space (assigned memory base + offset).  
 MethodLockResource Locks the resource for this session with an exclusive lock, with an infinite timeout. (Inherited from Ivi.Visa.IVisaSession)
 MethodMapAddress Map the specified memory space into this process’s address space.  
 MethodMoveIn16Overloaded.  Move a 16-bit block of data from the specified memory space (assigned memory base + offset) to local memory.  
 MethodMoveIn32Overloaded.  Move a 32-bit block of data from the specified memory space (assigned memory base + offset) to local memory.  
 MethodMoveIn64Overloaded.  Move a 64-bit block of data from the specified memory space (assigned memory base + offset) to local memory.  
 MethodMoveIn8Overloaded.  Move an 8-bit block of data from the specified memory space (assigned memory base + offset) to local memory.  
 MethodMoveOut16Overloaded.  Moves an 16-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset).  
 MethodMoveOut32Overloaded.  Moves an 32-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset).  
 MethodMoveOut64Overloaded.  Moves an 64-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset).  
 MethodMoveOut8Overloaded.  Moves an 8-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset).  
 MethodOut16 Write a 16-bit value to the specified memory space (assigned memory base + offset).  
 MethodOut32 Write a 32-bit value to the specified memory space (assigned memory base + offset).  
 MethodOut64 Write a 64-bit value to the specified memory space (assigned memory base + offset).  
 MethodOut8 Write an 8-bit value to the specified memory space (assigned memory base + offset).  
 MethodUnlockResource Unlock the resource. (Inherited from Ivi.Visa.IVisaSession)
 MethodWaitOnEventWait for events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
Top
See Also

Reference

IRegisterBasedSession Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025