Keysight VISA.NET Help
UsbInterfaceNumber Property (IUsbSession)



The USB interface number of the interface to which the USB device is connected.
Syntax
'Declaration
 
ReadOnly Property UsbInterfaceNumber As Short
'Usage
 
Dim instance As IUsbSession
Dim value As Short
 
value = instance.UsbInterfaceNumber
short UsbInterfaceNumber {get;}
property short UsbInterfaceNumber {
   short get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025