Keysight VISA.NET Help
FastDataChannelNumber Property (IVxiSession)



The FDC channel that will be used when transferring data.
Syntax
'Declaration
 
Property FastDataChannelNumber As Short
'Usage
 
Dim instance As IVxiSession
Dim value As Short
 
instance.FastDataChannelNumber = value
 
value = instance.FastDataChannelNumber
short FastDataChannelNumber {get; set;}
property short FastDataChannelNumber {
   short get();
   void set (    short value);
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025