Keysight VISA.NET Help
AliasIfExists Property



Specifies the user-defined alias for the given resourcestring, if a VISA implementation allows aliases and an alias exists for the given resource string.
Syntax
'Declaration
 
Public ReadOnly Property AliasIfExists As String
'Usage
 
Dim instance As ParseResult
Dim value As String
 
value = instance.AliasIfExists
public string AliasIfExists {get;}
public:
property String^ AliasIfExists {
   String^ get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025