Keysight VISA.NET Help
VisaConstants Class Members
Fields 


The following tables list the members exposed by VisaConstants.

Public Fields
 NameDescription
Public FieldGpibNoSecondaryAddress For GPIB resources, this value indicates that there is no secondary address. Actual secondary address values are in the range 0-30 inclusive.  
Public FieldImmediateTimeout Specifies an immediate timeout, for use with method overloads where the timeout is specified in milliseconds. If the operation cannot be satisfied immediately, it throws a timeout exception rather than blocking.  
Public FieldInfiniteTimeout Specifies an infinite timeout, for use with method overloads where the timeout is specified in milliseconds.  
Public FieldUnknownSlotNumber For PXI and VXI resources, this value indicates that the slot number is unknown or not applicable.  
Public FieldVxiUnknownLogicalAddress For VXI and VME resources, this value indicates that the logical address is unknown or not applicable.  
Top
See Also

Reference

VisaConstants Class
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025