Keysight VISA.NET Help
Keysight.Visa Assembly

The Keysight.Visa assembly contains the Keysight VISA.NET implementation, including support for all of the session interfaces defined in the IVI VISA.NET interfaces.

The Keysight.Visa assembly contains one namespace, Keysight.Visa, which includes the entire implementation.

A Note on Versioning 

Most future versions of the Keysight.Visa assembly will automatically use assembly policy files to policy up (that is, redirect) references to earlier version of the assembly to the latest version without rebuilding client programs. You can use application policy files to continue to reference older versions if needed. In the very rare case where there are breaking changes that make this impossible, the Keysight IO Libraries Suite readme file will notify you that you must manually update code to the latest version and rebuild.

 

Namespaces
NamespaceDescription
Keysight.VisaThe Keysight.Visa namespace contains the Keysight implementation of the IVI Foundation standard VISA.NET API.

 

 


© Keysight Technologies 2015-2025