| Keysight.Visa Namespace > GpibInterfaceSession Class : ControlAtn Method |
'UsageDim instance As GpibInterfaceSession Dim command As AtnMode instance.ControlAtn(command)
This operation asserts or deasserts the GPIB ATN interface line according to the specified mode. The mode can also specify whether the local interface board should acquire or release Controller Active status.
It is generally not necessary to use the viGpibControlATN operation in most applications. Other methods such as PassControl and SendCommand modify the ATN and/or CIC state automatically.
Current with Keysight IO Libraries Suite 18