Keysight VISA.NET Help
SendInterfaceClear Method (GpibInterfaceSession)



Pulses the interface clear line (IFC) for at least 100 microseconds. This operation asserts the IFC line and the local interface becomes controller in charge (CIC).
Syntax
'Declaration
 
Public Sub SendInterfaceClear() 
'Usage
 
Dim instance As GpibInterfaceSession
 
instance.SendInterfaceClear()
public void SendInterfaceClear()
public:
void SendInterfaceClear(); 
Remarks

The local board must be the system controller.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025