| Keysight.Visa Namespace : KeysightVisaEventArgs Class |
The following tables list the members exposed by KeysightVisaEventArgs.
| Name | Description | |
|---|---|---|
![]() | KeysightVisaEventArgs Constructor | Initializes a new instance of the KeysightVisaEventArgs class. |
| Name | Description | |
|---|---|---|
![]() | EventArgs | An event args reference for the native C event. This may reference an object that derives from EventArgs, if the event handler for the event specified by the EventArg.EventType of EventArg.CustomEventType properties uses a derived class. |
![]() | EventContextHandle | An event args reference for the native C event. This may reference an object that derives from EventArgs, if the event handler for the event specified by the EventArg.EventType of EventArg.CustomEventType properties uses a derived class. |
| Name | Description | |
|---|---|---|
![]() | Dispose | Overloaded. Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this event arguments object, but only if another thread has not already started to dispose of the object. |
![]() | GetAttributeBoolean | Overloaded. Retrieves the value of the specified attribute from the native C implementation. |
![]() | GetAttributeByte | Overloaded. Retrieves the value of the specified attribute from the native C implementation. |
![]() | GetAttributeInt16 | Overloaded. Retrieves the value of the specified attribute from the native C implementation. |
![]() | GetAttributeInt32 | Overloaded. Retrieves the value of the specified attribute from the native C implementation. |
![]() | GetAttributeInt64 | Overloaded. Retrieves the value of the specified attribute from the native C implementation. |
![]() | GetAttributeString | Overloaded. Retrieves the value of the specified attribute from the native C implementation. |