Keysight VISA.NET Help
AssertTrigger Method (MessageBasedSession)



Asserts a software or hardware trigger, depending on the default trigger protocol for the session type.
Syntax
'Declaration
 
Public Sub AssertTrigger() 
'Usage
 
Dim instance As MessageBasedSession
 
instance.AssertTrigger()
public void AssertTrigger()
public:
void AssertTrigger(); 
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025