Keysight VISA.NET Help
MapTrigger Method (PxiBackplaneSession)



Maps the specified source trigger line to the specified destination trigger line.
Overload List
OverloadDescription
MapTrigger(Int16,TriggerLine,Int16,TriggerLine) Maps the specified source trigger line to the specified destination trigger line.  
MapTrigger(Int16,TriggerLine,Int16,TriggerLine,Boolean) Maps the specified source trigger line to the specified destination trigger line.  
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025