Keysight VISA.NET Help
PxiMemorySession Class Members
Properties  Methods 


The following tables list the members exposed by PxiMemorySession.

Public Constructors
 NameDescription
Public ConstructorPxiMemorySession ConstructorOverloaded.   
Top
Public Properties
 NameDescription
Public PropertyAllowDma Specifies whether direct memory access is enabled. (Inherited from Keysight.Visa.RegisterBasedSession)
Public PropertyDestinationIncrement For MoveOut methods, specifies whether to do a block move or a FIFO read. (Inherited from Keysight.Visa.RegisterBasedSession)
Public PropertyEventQueueCapacity The maximum number of events that can be queued at any time on this session. The default is 50. (Inherited from Keysight.Visa.VisaSession)
Public PropertyExportEnabledTogether with the Keysight ResourceManager.FindExportedResourcesOnly property, determines whether the resource associated with this session instance is reported by the Keysight ResourceManager.Find and ResourceManager.Parse methods. (Inherited from Keysight.Visa.VisaSession)
Public PropertyHardwareInterfaceName A human-readable description of the hardware interface associated with this session. (Inherited from Keysight.Visa.VisaSession)
Public PropertyHardwareInterfaceNumber The board number of the hardware interface associated with this session. (Inherited from Keysight.Visa.VisaSession)
Public PropertyHardwareInterfaceType The type (GPIB, ASRL, etc.) of the hardware interface associated with this session. (Inherited from Keysight.Visa.VisaSession)
Public PropertyInternalHandle The VISA C handle to the underlying VISA C session. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceClass The resource class of the currently open resource. Possible values are INSTR, INTFC, MEMMAC, SOCKET, and BACKPLANE. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceImplementationVersion The version of this Keysight VISA.NET implementation. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceLockState The state of the resource-wide lock on the currently open resource. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceManagerA private instance of the ResourceManager created when this session was instantiated, and available until this session is disposed. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceManufacturerId The VXI manufacturer ID of the software vendor of this VISA.NET implementation - '4095'. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceManufacturerName The name of the software vendor that corresponds to the ResourceManufacturerId property - 'Keysight Technologies, Inc.'. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceName The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resourceName parameter used to instantiate the session. (Inherited from Keysight.Visa.VisaSession)
Public PropertyResourceSpecificationVersion The version of the VISA.NET specification that describes the functionality provided by this session class. (Inherited from Keysight.Visa.VisaSession)
Public PropertySessionType The type of the current session. (Inherited from Keysight.Visa.VisaSession)
Public PropertySourceIncrement For MoveIn methods, specifies whether to do a block move or a FIFO read. (Inherited from Keysight.Visa.RegisterBasedSession)
Public PropertySynchronizeCallbacks Specifies whether callbacks must be performed in a specific synchronization context. If false, the implementation is allowed to execute callbacks in any context. The default value is true. This property applies to this session only (local scope). (Inherited from Keysight.Visa.VisaSession)
Public PropertyTimeoutMilliseconds The I/O timeout in milliseconds for I/O communication on this resource session. (Inherited from Keysight.Visa.VisaSession)
Public PropertyWaitForLockRelease Indicates whether methods and properties from this session instance will wait for a timeout period for a resource lock to be released (true) or not (false). (Inherited from Keysight.Visa.VisaSession)
Top
Public Methods
 NameDescription
Public MethodDisableEventDisables a calling program's ability to receive events of the type specified by the eventType argument using a VisaSession.WaitOnEvent method (any overload). (Inherited from Keysight.Visa.VisaSession)
Public MethodDiscardEventsDiscards events of the type specified by the eventType argument from the queue for that event type. (Inherited from Keysight.Visa.VisaSession)
Public MethodDisposeOverloaded.  Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession)
Public MethodEnableEventEnables a calling program's ability to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Keysight.Visa.VisaSession)
Public MethodIn16 Reads in a 16-bit value from the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodIn32 Reads in a 32-bit value from the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodIn64 Reads in a 64-bit value from the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodIn8 Read in an 8-bit value from the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodLockResourceOverloaded.  Acquires a lock on the resource for this session. (Inherited from Keysight.Visa.VisaSession)
Public MethodMapAddress Maps the specified memory space into this process’s address space. (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMemoryAllocateOverloaded.  Allocates memory from the device’s memory region.  
Public MethodMemoryFree Frees previously-allocated memory.  
Public MethodMoveIn16Overloaded.  Moves a 16-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveIn32Overloaded.  Moves a 32-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveIn64Overloaded.  Moves a 64-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveIn8Overloaded.  Moves an 8-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveOut16Overloaded.  Moves an 16-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveOut32Overloaded.  Moves an 32-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveOut64Overloaded.  Moves an 64-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodMoveOut8Overloaded.  Moves an 8-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodOut16 Writes a 16-bit value to the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodOut32 Writes a 32-bit value to the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodOut64 Writes a 64-bit value to the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodOut8 Writes an 8-bit value to the specified memory space (assigned memory base + offset). (Inherited from Keysight.Visa.RegisterBasedSession)
Public MethodUnlockResource Unlocks the resource. (Inherited from Keysight.Visa.VisaSession)
Public MethodWaitOnEventOverloaded.  Waits for an occurrence of the specified event for this session. In particular, WaitOnEvent suspends execution of the thread on which it is called and waits for the specified event indefinitely. (Inherited from Keysight.Visa.VisaSession)
Top
Protected Methods
 NameDescription
Protected MethodFinalize Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession)
Top
See Also

Reference

PxiMemorySession Class
Keysight.Visa Namespace

 

 


© Keysight Technologies 2015-2025