Keysight VISA.NET Help
ReadTermination Property (SerialSession)



The method used to terminate read operations.
Syntax
'Declaration
 
Public Property ReadTermination As SerialTerminationMethod
'Usage
 
Dim instance As SerialSession
Dim value As SerialTerminationMethod
 
instance.ReadTermination = value
 
value = instance.ReadTermination
public SerialTerminationMethod ReadTermination {get; set;}
public:
property SerialTerminationMethod ReadTermination {
   SerialTerminationMethod get();
   void set (    SerialTerminationMethod value);
}
Remarks

The default is Ivi.Visa.SerialTerminationMethod.TerminationCharacter.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025