Keysight VISA.NET Help
ReplacementCharacter Property (SerialSession)



The character used to replace incoming characters that arrive with errors (such as parity errors).
Syntax
'Declaration
 
Public Property ReplacementCharacter As Byte
'Usage
 
Dim instance As SerialSession
Dim value As Byte
 
instance.ReplacementCharacter = value
 
value = instance.ReplacementCharacter
public byte ReplacementCharacter {get; set;}
public:
property byte ReplacementCharacter {
   byte get();
   void set (    byte value);
}
Remarks

The range is between 0 and Byte.MaxValue, inclusive. The default is 0.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025