| | Name | Description |
 | Address |
The TCP/IP address of the device to which the session is connected, formatted in
dot-notation.
|
 | EventQueueCapacity |
The maximum number of events that can be queued at any time on this session. The default
is 50.
(Inherited from Keysight.Visa.VisaSession) |
 | ExportEnabled | Together with the Keysight ResourceManager.FindExportedResourcesOnly property, determines whether the resource associated with this session instance is reported by the Keysight Find and Parse methods. (Inherited from Keysight.Visa.VisaSession) |
 | FormattedIO |
A reference to the Formatted I/O interface. Keysight VISA.NET uses the standard Formatted
I/O implementation provided by the IVI Foundation in the VISA.NET Shared Components.
(Inherited from Keysight.Visa.MessageBasedSession) |
 | HardwareInterfaceName |
A human-readable description of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceNumber |
The board number of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceType |
The type (GPIB, ASRL, etc.) of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HostName |
The host name of the device. If no host name is available, this property is set to the
empty string.
|
 | InternalHandle |
The VISA C handle to the underlying VISA C session.
(Inherited from Keysight.Visa.VisaSession) |
 | IOProtocol |
The protocol type for I/O communication with the device. This property applies to this
session only (VISA local scope).
(Inherited from Keysight.Visa.MessageBasedSession) |
 | KeepAlive |
If true, the TCP/IP provider enables the use of keep-alive packets on TCP connections.
|
 | NoDelay |
If true, the Nagle algorithm is disabled.
|
 | Port |
The port number for a given TCP/IP address (required for a TCP/IP SOCKET resource).
|
 | RawIO |
A reference to the raw (no formatting) I/O interface.
(Inherited from Keysight.Visa.MessageBasedSession) |
 | ResourceClass |
The resource class of the currently open resource. Possible values are INSTR, INTFC, MEMMAC,
SOCKET, and BACKPLANE.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceImplementationVersion |
The version of this Keysight VISA.NET implementation.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceLockState |
The state of the resource-wide lock on the currently open resource.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceManager | A private instance of the ResourceManager created when this session was instantiated, and available until this session is disposed. (Inherited from Keysight.Visa.VisaSession) |
 | ResourceManufacturerId |
The VXI manufacturer ID of the software vendor of this VISA.NET implementation - '4095'.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceManufacturerName |
The name of the software vendor that corresponds to the ResourceManufacturerId property -
'Keysight Technologies, Inc.'.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceName |
The VISA resource name of the currently open resource. This name is the canonical version
of the resource name and therefore may vary from the resourceName parameter used to
instantiate the session.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceSpecificationVersion |
The version of the VISA.NET specification that describes the functionality provided by this
session class.
(Inherited from Keysight.Visa.VisaSession) |
 | SendEndEnabled |
Enables/disables sending the END signal on the last byte of a write. This property applies
to this session only (VISA local scope).
(Inherited from Keysight.Visa.MessageBasedSession) |
 | ServerCertificate |
The full text of the server certificate in RFC 5652 PEM format.
|
 | ServerCertificateExpirationDate |
The expiration date of the server certificate in UTC.
|
 | ServerCertificateIsPerpetual |
Indicates the certificate does not expire. Note that this may indicate that the certificate is from an IDevID.
|
 | ServerCertificateIssuerName |
The name of the CA that signed the certificate.
For an IDevId, this will indicate the name of the PKI CA.
|
 | ServerCertificateSubjectName |
The subject field from the certificate.
That is, the entity associated with the public key in the certificate.
|
 | SessionType |
The type of the current session.
(Inherited from Keysight.Visa.VisaSession) |
 | SynchronizeCallbacks |
Specifies whether callbacks must be performed in a specific synchronization context. If false,
the implementation is allowed to execute callbacks in any context. The default value is true.
This property applies to this session only (local scope).
(Inherited from Keysight.Visa.VisaSession) |
 | TerminationCharacter | The ASCII character used to end reading. This property applies to this session only (VISA local scope). (Inherited from Keysight.Visa.MessageBasedSession) |
 | TerminationCharacterEnabled | If true, read operations end when a termination character is received. This property applies to this session only (VISA local scope). (Inherited from Keysight.Visa.MessageBasedSession) |
 | TimeoutMilliseconds |
The I/O timeout in milliseconds for I/O communication on this resource session.
(Inherited from Keysight.Visa.VisaSession) |
 | TlsCipherSuite |
A string that indicates the cipher suite used by TLS, which tells the user something about the security of the connection.
For details, refer to https://www.iana.org/assignments/tls-parameters/tls-parameters.xml.
For example, TLS_ECDHE_RSA_WITH_AES_256_GCM_SHA384.
|
 | WaitForLockRelease |
Indicates whether methods and properties from this session instance will wait for a timeout
period for a resource lock to be released (true) or not (false).
(Inherited from Keysight.Visa.VisaSession) |