| Keysight.Visa Namespace > VxiBackplaneSession Class : ChassisLogicalAddress Property |
'DeclarationPublic ReadOnly Property ChassisLogicalAddress As Short
'UsageDim instance As VxiBackplaneSession Dim value As Short value = instance.ChassisLogicalAddress
public short ChassisLogicalAddress {get;}
The range is between 0 and 255, inclusive.
This is the logical address of a given device in the mainframe, usually the device with the lowest logical address. Other possible values include the logical address of the Slot 0 controller or of the parent-side extender. Often, these are all the same value.
Since the purpose of this attribute is to provide a unique ID for each mainframe, a VISA manufacturer can choose any of these values, but must be consistent across mainframes.
The value Ivi.Visa.VisaConstants.VxiUnknownLogicalAddress (-1) indicates that a chassis logical address cannot be determined.
Current with Keysight IO Libraries Suite 18