Keysight VISA.NET Help
MapTrigger(TriggerLine,TriggerLine,Boolean) Method



The source trigger line.
The destination trigger line.
If true, the trigger has already been mapped.
Map the specified source trigger line to the specified destination trigger line.
Syntax
'Declaration
 
Public Overloads Sub MapTrigger( _
   ByVal sourceLine As TriggerLine, _
   ByVal destinationLine As TriggerLine, _
   ByRef alreadyMapped As Boolean _
) 
'Usage
 
Dim instance As VxiBackplaneSession
Dim sourceLine As TriggerLine
Dim destinationLine As TriggerLine
Dim alreadyMapped As Boolean
 
instance.MapTrigger(sourceLine, destinationLine, alreadyMapped)

Parameters

sourceLine
The source trigger line.
destinationLine
The destination trigger line.
alreadyMapped
If true, the trigger has already been mapped.
Remarks

Mapping a trigger line (as either source or destination) multiple times requires special hardware capabilities and is not guaranteed to be implemented.

If this operation is called multiple times on the same backplane resource with the same source trigger line and different destination trigger lines, the result should be that when the source trigger line is asserted all specified destination trigger lines should also be asserted.

If this operation is called multiple times on the same backplane resource with different source trigger lines and the same destination trigger line the result should be that when any of the specified source trigger lines is asserted, the destination trigger line should also be asserted.

Mapping one trigger line to another modifies the state of hardware. Therefore, the effect continues beyond the scope of the VISA.NET session that mapped it, even if that VISA.NET session is closed.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025