| | Name | Description |
 | AllowDma |
Specifies whether direct memory access is enabled.
(Inherited from Keysight.Visa.RegisterBasedSession) |
 | DestinationIncrement |
For MoveOut methods, specifies whether to do a block move or a FIFO read.
(Inherited from Keysight.Visa.RegisterBasedSession) |
 | EventQueueCapacity |
The maximum number of events that can be queued at any time on this session. The default
is 50.
(Inherited from Keysight.Visa.VisaSession) |
 | ExportEnabled | Together with the Keysight ResourceManager.FindExportedResourcesOnly property, determines whether the resource associated with this session instance is reported by the Keysight Find and Parse methods. (Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceName |
A human-readable description of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceNumber |
The board number of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceType |
The type (GPIB, ASRL, etc.) of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | InternalHandle |
The VISA C handle to the underlying VISA C session.
(Inherited from Keysight.Visa.VisaSession) |
 | LogicalAddress |
The logical address of the VXI or VME controller for this interface.
|
 | ResourceClass |
The resource class of the currently open resource. Possible values are INSTR, INTFC, MEMMAC,
SOCKET, and BACKPLANE.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceImplementationVersion |
The version of this Keysight VISA.NET implementation.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceLockState |
The state of the resource-wide lock on the currently open resource.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceManager | A private instance of the ResourceManager created when this session was instantiated, and available until this session is disposed. (Inherited from Keysight.Visa.VisaSession) |
 | ResourceManufacturerId |
The VXI manufacturer ID of the software vendor of this VISA.NET implementation - '4095'.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceManufacturerName |
The name of the software vendor that corresponds to the ResourceManufacturerId property -
'Keysight Technologies, Inc.'.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceName |
The VISA resource name of the currently open resource. This name is the canonical version
of the resource name and therefore may vary from the resourceName parameter used to
instantiate the session.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceSpecificationVersion |
The version of the VISA.NET specification that describes the functionality provided by this
session class.
(Inherited from Keysight.Visa.VisaSession) |
 | SessionType |
The type of the current session.
(Inherited from Keysight.Visa.VisaSession) |
 | SourceIncrement |
For MoveIn methods, specifies whether to do a block move or a FIFO read.
(Inherited from Keysight.Visa.RegisterBasedSession) |
 | SynchronizeCallbacks |
Specifies whether callbacks must be performed in a specific synchronization context. If false,
the implementation is allowed to execute callbacks in any context. The default value is true.
This property applies to this session only (local scope).
(Inherited from Keysight.Visa.VisaSession) |
 | TimeoutMilliseconds |
The I/O timeout in milliseconds for I/O communication on this resource session.
(Inherited from Keysight.Visa.VisaSession) |
 | WaitForLockRelease |
Indicates whether methods and properties from this session instance will wait for a timeout
period for a resource lock to be released (true) or not (false).
(Inherited from Keysight.Visa.VisaSession) |