Keysight VISA.NET Help
DeviceClass Property (VxiSession)



The VXI-defined device class to which the resource belongs.
Syntax
'Declaration
 
Public ReadOnly Property DeviceClass As VxiDeviceClass
'Usage
 
Dim instance As VxiSession
Dim value As VxiDeviceClass
 
value = instance.DeviceClass
public VxiDeviceClass DeviceClass {get;}
public:
property VxiDeviceClass DeviceClass {
   VxiDeviceClass get();
}
Remarks

VME devices are usually either register based (Register) or belong to a miscellaneous class (Other).

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025