Keysight VISA.NET Help
MemoryMapAccessPrivilege Property (VxiSession)



[Register-Based] The address modifier to be used in Ivi.Visa.IMemoryMap operations when accessing the mapped window.
Syntax
'Declaration
 
Public Property MemoryMapAccessPrivilege As VxiAccessPrivilege
'Usage
 
Dim instance As VxiSession
Dim value As VxiAccessPrivilege
 
instance.MemoryMapAccessPrivilege = value
 
value = instance.MemoryMapAccessPrivilege
public VxiAccessPrivilege MemoryMapAccessPrivilege {get; set;}
public:
property VxiAccessPrivilege MemoryMapAccessPrivilege {
   VxiAccessPrivilege get();
   void set (    VxiAccessPrivilege value);
}
Remarks

The default is DataPrivileged.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025