Keysight VISA.NET Help
Reading Integers

Reading Integers

An integer argument has a format specifier in one of the following forms:

d[*|@[1|H|Q|B]][width][,[arraySize]]d

i[*|@[1|H|Q|B]][width [,[arraySize]]i

u[*|@[1|H|Q|B]][width][,[arraySize]]u

o[*|@[Q|B]][width][,[arraySize]]o

x[*|@[H|B]][width][,[arraySize]]x

X[*|@[H|B]][width][,[arraySize]]X

Modifier

Interpretation

Default Functionality

The data in the read buffer is parsed as an integer or array of integers. 

flags

*

@1

@H, @Q, @B

Controls parsing, as follows:

  • '*' indicates that the data is to be parsed and skipped - there is no corresponding output argument in the Scanf call.
  • '@1' parses the value using the IEEE 488.2 NR1 format.
  • '@H' parses the value using the IEEE 488.2 hexadecimal format.
  • '@Q' parses the value using the IEEE 488.2 octal format.
  • '@B' parses the value using the IEEE 488.2 binary format.

width

The maximum number of characters to be parsed for this specifier.

A hash character (#) may be present in lieu of an integer width modifier, in which case the value is specified in the Scanf inputs array argument.

,[arraySize]

Parse a comma-separated array of integers.  If arraySize is specified, it is the maximum number of elements to include in the formatted array.

A hash character (#) may be present in lieu of an integer arraySize modifier, in which case the value is specified in the Scanf inputs array argument. 

Integer Parsing Code Snippets

Remember that Scanf is reading bytes from the formatted read buffer, parsing them according to the format specifiers, and placing the results in an output variable. The comment preceding each line shows the data being parsed by the snippet and the resulting value that is returned in the corresponding output argument, like this: //  "<data to parse>",  "<value>".  The <value> may optionally be followed by a comment in parentheses.

Assume that the io variable is a valid reference to IMessageBasedFormattedIO.  Assume that resultn is an out argument declared as a .NET signed integer.  Any size integer type is capable of holding any of the integers used in these snippets.

No Modifiers
Copy Code
// "8, -16, 32\n", 8, -16, 32
io.Scanf("%d, %i, %u\n", out result1, result2, result3);
 
// "17, f, 1A\n", 15, 15, 26
io.Scanf("%o, %x, %X\n", out result1, result2, result3);
Flags
Copy Code
// "13, 17, f, 1A\n", 15, 15, 26
io.Scanf("%*o, %o, %x, %X\n", out result1, result2, result3);
IEEE 488.2 Format Modifiers
Copy Code
// "123\n", 123
io.Scanf("@1d*t", out result1);
// "#B110110\n", 54
io.Scanf("@Bd*t", out result1);
// "#Q14\n", 12
io.Scanf("@Qd*t", out result1);
// "#H1A\n", 26
io.Scanf("@HX*t", out result1);
Width Modifier
Copy Code
// "123456\n", 12
io.Scanf("2d*T", out result1);
 
// "123456\n", 12
io.Scanf("#d*T", new Int64[] {2}, out result1);

The following two snippets demonstrate a known issue with width and the IEEE @H, @Q, and @B flags.  Note that in the first snippet, Scanf correctly uses the width of 4 to read and parse "0X1A" from the response.  In the second snippet, Scanf does not count the initial "#H" against the width, and so a width of 2 is used to parse "#H1A" so that 26 is returned.

Known Issue
Copy Code
// "0X1AFFF\n", 26
io.Scanf("4X*T", out result1);
 
// "#H1AFFF\n", 26
io.Scanf("@H2X*T", out result1);
ScanfArray
Copy Code
// "1, 2, 3, 4\n", { 1, 2, 3, 4 } - Memory must be allocated by the calling program.
Int32[10] out1;
io.ScanfArray("%,d%*T", out1);

 

 


© Keysight Technologies 2015-2026