Getting Started with VISA
This section contains information specific to the Windows product.
The VISA C DLL (visa32.dll) has a number of entry points that implement C-style function calls for doing VISA operations, primarily reading and writing data from/to instruments. While these entry points were designed primarily for use in the C/C++ languages, a number of other languages provide facilities for calling C-style DLLs. One of the these languages is Microsoft's Visual Basic 6 (VB6). The header file for that language, visa32.bas, allows access to most of VISA's functions, but with severe limitations to the formatted I/O functions such as viPrintf and viScanf due to limitations of the VB6 interoperability features.
The functions appear in VB .NET as a number of empty functions inside a Friend Module. In C# they appear as static methods inside an internal sealed class that never needs instantiation. They are declared with friend/internal access, so that any libraries that include them will not accidentally export the VISA definitions. The functions are a set of stubs that call out to the VISA C DLL at runtime. At development time, the only thing that the .NET environment knows about them is what is in the header files. There is no equivalent of a .lib file in .NET.
This tutorial demonstrates Keysight-defined header files for C# and VB .NET, two languages that have the ability to call into C DLLs. These header files provide some access to the formatted I/O functions, and they can be extended to do anything that could be done in C/C++.
Next: Creating Your Project