Using the VISA C API in Microsoft .NET
                                            
 Support for .NET is a Windows-only feature.
Test and measurement programmers accustomed to using the VISA C API (implemented by the visa32.dll C DLL) for communicating with instruments are familiar with the visa32.h C standard header file for use in C and C++. This header file is defined by the VXIplug&play Systems Alliance and distributed by Keysight Technologies, among others. The alliance also defines a header file visa32.bas for Microsoft Visual Basic 6. However, there are at present no officially defined header files for programming in the VISA C API in the Microsoft .NET technology languages, such as C# and Visual Basic .NET.
Keysight defines and provides header files to allow programmatic access to the VISA C API from the two most popular .NET languages. This document describes Keysight's .NET header files for VISA, VISA32.cs for C# and VISA32.vb for VB .NET; provides examples for some of the methods; and provides a tutorial for using VISA in these languages.
Programmers wishing to use the VISA C API in .NET must include the appropriate header file in their projects. The compiled .NET assemblies will then have all the information they need to use the VISA C Library (visa32.dll). The Tutorial shows how to include and compile a program using these header files.
This help is broken into several topics following the introduction. The first, VISA API Essentials, lists the core set of methods you need to communicate with instruments through Keysight's .NET header files for VISA. Follow the links into the reference for those methods to see .NET examples in C# and VB .NET. The second section, Tutorial, provides a brief tutorial in both C# and VB .NET describing a complete use of the header files from start to finish. The third section, Advanced Use of viPrintf/viScanf, describes how to add parameters and make your own versions of the functions. The last section, .NET Types and VISA C Types Reference, describes the translation of the C VISA data types to .NET and provides a conversion table.