TCPIP Socket (SOCKET) Resource
This topic describes the TCPIP Socket (SOCKET) Resource that encapsulates the operations and properties of the capabilities of a raw network socket connection using TCPIP.
SOCKET Resource Overview
A VISA SOCKET Resource, like any other resource, starts with the basic operations and attributes of the VISA Resource Template. For example, modifying the state of an attribute is done via the operation viSetAttribute, which is defined in the VISA Resource Template.
Although the TCPIP resource does not have viSetAttribute listed in its operations, it provides the operation because it is defined in the VISA Resource Template. From this basic set, each resource adds its specific operations and attributes that allow it to perform its dedicated task.
The SOCKET Resource exposes the capability of a raw network socket connection over TCPIP. This usually means Ethernet, but the protocol is not restricted to that physical interface. Services are provided to send and receive blocks of data. If the device is capable of communicating with IEEE-488.2-style strings, an attribute setting also allows sending software triggers, querying an IEEE-488-style status byte, and sending a device clear message.
SOCKET Resource Attributes
AP = Access Privileges
|
Attribute Name |
Attribute Value |
Access Privilege |
Data Type |
Range |
Default |
|
|---|---|---|---|---|---|---|
Generic SOCKET Resource Attributes |
||||||
| 0x3FFF001EUL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_FALSE |
|
| 0x3FFF0192UL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_FALSE |
|
| 0xBFFF00E9UL |
RO |
Global |
ViString |
N/A |
N/A |
|
| 0x3FFF0176UL |
RO |
Global |
ViUInt16 |
0 to FFFFh |
0 |
|
| 0x3FFF0171UL |
RO |
Global |
ViUInt16 |
VI_INTF_TCPIP |
VI_INTF_TCPIP |
|
| 0x3FFF001CUL |
RW |
Local |
ViUInt16 |
VI_NORMAL |
VI_PROT_4882_STRS |
|
| 0x3FFF002AUL |
RW |
Local |
ViUInt16 |
VI_FLUSH_ON_ACCESS |
VI_FLUSH_DISABLE |
|
| 0x3FFF0016UL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_TRUE |
|
| 0x3FFF0018UL |
RW |
Local |
ViUInt8 |
0 to FFh |
0Ah(linefeed) |
|
| 0x3FFF0038UL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_FALSE |
|
| 0x3FFF001AUL |
RW |
Local |
ViUInt32 |
VI_TMO_IMMEDIATE |
2000 msec. |
|
| 0x3FFF002DUL |
RW |
Local |
ViUInt16 |
VI_FLUSH_ON_ACCESS |
VI_FLUSH_WHEN_FULL |
|
| 0x3FFF002BUL |
RO |
Local |
ViUInt32 |
N/A |
N/A |
|
| 0x3FFF002EUL |
RO |
Local |
ViUInt32 |
N/A |
N/A |
|
TCPIP Specific SOCKET Resource Attributes |
||||||
| 0xBFFF0195UL |
RO |
Global |
ViString |
N/A |
N/A |
|
| 0xBFFF0196UL |
RO |
Global |
ViString |
N/A |
N/A |
|
| 0x3FFF0197UL |
RO |
Global |
ViUInt16 |
0 to FFFFh |
N/A |
|
| 0x3FFF019AUL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_TRUE |
|
| 0x3FFF019BUL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_FALSE |
|
SOCKET Resource Attribute Descriptions
|
Attribute Name |
Description |
|---|---|
Generic SOCKET Resource Attributes |
|
|
VI_ATTR_DMA_ALLOW_EN |
This attribute specifies whether I/O accesses should use DMA ( VI_TRUE) or Programmed I/O ( VI_FALSE). In some implementations, this attribute may have global effects even though it is documented to be a local attribute. Since this affects performance and not functionality, that behavior is acceptable. |
|
VI_ATTR_FILE_APPEND_EN |
This attribute specifies whether viReadToFile will overwrite (truncate) or append when opening a file. |
|
VI_ATTR_INTF_INST_NAME |
Human-readable text describing the given interface. |
|
VI_ATTR_INTF_NUM |
Board number for the given interface. |
|
VI_ATTR_INTF_TYPE |
Interface type of the given session. |
|
VI_ATTR_IO_PROT |
Specifies which protocol to use. |
|
VI_ATTR_RD_BUF_OPER_MODE |
Determines the operational mode of the read buffer. When the operational mode is set to VI_FLUSH_DISABLE (default), the buffer is flushed only on explicit calls to viFlush. |
|
VI_ATTR_SEND_END_EN |
Whether to assert END during the transfer of the last byte of the buffer. |
|
VI_ATTR_TERMCHAR |
Termination character. When the termination character is read and VI_ATTR_TERMCHAR_EN is enabled during a read operation, the read operation terminates. Note: the termination character must be enabled in the program when reading from a SOCKET device that does not support EOI; otherwise the SOCKET read will timeout. |
|
VI_ATTR_TERMCHAR_EN |
Flag that determines whether the read operation should terminate when a termination character is received. |
|
VI_ATTR_TMO_VALUE |
Minimum timeout value to use, in milliseconds. A timeout value of VI_TMO_IMMEDIATE means that operations should never wait for the device to respond. A timeout value of VI_TMO_INFINITE disables the timeout mechanism. |
|
VI_ATTR_WR_BUF_OPER_MODE |
Determines the operational mode of the write buffer. When the operational mode is set to VI_FLUSH_WHEN_FULL (default), the buffer is flushed when an END indicator is written to the buffer or when the buffer fills up. If the operational mode is set to VI_FLUSH_ON_ACCESS, the write buffer is flushed under the same conditions, and also every time a viPrintf operation completes. |
|
VI_ATTR_RD_BUF_SIZE |
This attribute specifies the size of the formatted I/O read buffer. The user can modify this value by calling viSetBuf(). |
|
VI_ATTR_WR_BUF_SIZE |
This attribute specifies the size of the formatted I/O write buffer. The user can modify this value by calling viSetBuf(). |
TCPIP Specific SOCKET Resource Attributes |
|
|
VI_ATTR_TCPIP_ADDR |
This is the TCPIP address of the device to which the session is connected. This string is formatted in dot notation. |
|
VI_ATTR_TCPIP_HOSTNAME |
Specifies the host name of the device. If no host name is available, this attribute returns an empty string. |
|
VI_ATTR_TCPIP_PORT |
Specifies the port number for a given TCPIP address. For a TCPIP SOCKET resource, this is a required part of the address string. |
|
VI_ATTR_TCPIP_NODELAY |
The Nagle algorithm is disabled when this attribute
is enabled (and vice versa). |
|
VI_ATTR_TCPIP_KEEPALIVE |
An application can request that a TCPIP provider enable the use of "keep-alive" packets on TCP connections by turning on this attribute. If a connection is dropped as a result of "keep-alives," the error code VI_ERROR_CONN_LOST is returned to current and subsequent I/O calls on the session. |
SOCKET Resource Event
This resource defines the following events for communication with applications, where AP = Access Privilege.
VI_EVENT_IO_COMPLETION - Notification that an asynchronous operation has completed.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
| 0x3FFF4027UL |
Address of a buffer that was used in an asynchronous operation. |
RO |
ViBuf |
N/A |
|
| 0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_IO_COMPLETION |
|
| 0x3FFF4006UL |
Job ID of the asynchronous operation that has completed. |
RO |
ViJobId |
N/A |
|
| 0xBFFF4042UL |
Name of the operation generating the event. |
RO |
ViString |
N/A |
|
| 0x3FFF4025UL |
Return code of the asynchronous I/O operation that has completed. |
RO |
ViStatus |
N/A |
|
|
32-bit: 0x3FFF4026UL 64-bit: 0x3FFF4028UL |
Actual number of elements that were asynchronously transferred. |
RO |
ViBus Size |
* |
|
| 0x3FFF4026UL |
Actual number of elements that were asynchronously transferred. |
RO |
ViUInt32 |
0 to FFFFFFFFh |
|
| 0x3FFF4028UL |
Actual number of elements that were asynchronously transferred. |
RO |
ViUInt64 |
0 to FFFFFFFF FFFFFFFFh |
*The data type is defined in the appropriate VPP 4.3.x framework specification.
**Defined only for operating systems that are 64-bit native.
SOCKET Resource Operations
viAssertTrigger (vi, protocol)
viBufRead (vi, buf, count, retCount)
viBufWrite (vi, buf, count, retCount)
viFlush (vi, mask)
viPrintf (vi, writeFmt, arg1, arg2, ...)
viRead (vi, buf, count, retCount)
viReadAsync (vi, buf, count, jobId)
viReadToFile (vi, filename, count, retCount)
viScanf (vi, readFmt, arg1, arg2, ...)
viSPrintf (vi, buf, writeFmt, arg1, arg2, ...)
viSScanf (vi, buf, readFmt, arg1, arg2, ...)
viVPrintf (vi, writeFmt, params)
viVScanf (vi, readFmt, params)
viVSPrintf (vi, buf, writeFmt, params)
viVSScanf (vi, buf, readFmt, params)
viWrite (vi, buf, count, retCount)