viAssertTrigger
Syntax
viAssertTrigger(ViSession vi, ViUInt16 protocol);
|
This function is not supported with the GPIB-VXI interface. |
Description
Assert software or hardware trigger. This operation will source a software or hardware trigger dependent on the interface type. For a GPIB device, the device is addressed to listen and then the GPIB GET command is sent.
For a VXI device, if VI_ATTR_TRIG_ID is VI_TRIG_SW, the device is sent the Word Serial Trigger command. For any other values of the attribute, a hardware trigger is sent on the line corresponding to the value of that attribute. For a GPIB device, if VI_ATTR_TRIG_ID is VI_TRIG_SW, the device is addressed to Listen and a Group Execute Trigger (GET) is sent.
For a serial session to a serial device or TCPIP socket, if VI_ATTR_IO_PROT is VI_PROT_4882_STRS, the device is sent the string "*TRG\n". Otherwise, this operation is not valid. For a session to a USB instrument, this function sends the TRIGGER message ID on the Bulk-OUT pipe.
For GPIB, ASRL, USB, and VXI software triggers, VI_TRIG_PROT_DEFAULT is the only valid protocol. For VXI hardware triggers, VI_TRIG_PROT_DEFAULT is equivalent to VI_TRIG_PROT_SYNC.
Keysight VISA applications operating PXI trigger line reservations/routes must be written to behave cooperatively by heeding the response status codes when reserving a trigger bus segment. If your application attempts to reserve a PXI trigger line and receives a returned status code indicating it is already reserved, then your application must conclude that there is another application that has reserved this line, and cooperate by avoiding use of that trigger line.
|
If a process does not release its trigger reservations or trigger routes, these reservations/routes will persist after the process ends. They will only be cleared when another application releases the reservations/routes, or when the PC is restarted. |
Keysight Connection Expert provides a Chassis Triggers view, which allows you to view existing trigger reservations/routes and make new reservations/routes (for the purposes of prototyping or troubleshooting). See the IO Libraries Suite Help (IO Control icon
> Documentation > IO Libraries Suite Help) for more information.
Parameters
|
Name |
Dir |
Type |
Description |
|---|---|---|---|
|
vi |
IN |
ViSession |
Unique logical identifier to a session. |
|
protocol |
IN |
ViUInt16 |
Trigger protocol to use during assertion. Valid values are: VI_TRIG_PROT_DEFAULT VI_TRIG_PROT_ON - asserts the trigger VI_TRIG_PROT_OFF - deasserts the trigger VI_TRIG_PROT_SYNC - pulses the trigger (assert followed by deassert) VI_TRIG_PROT_RESERVE - reserves the PXI trigger VI_TRIG_PROT_UNRESERVE - releases the PXI trigger reservation For GPIB, ASRL, USB, and VXI software triggers, VI_TRIG_PROT_DEFAULT is the only valid protocol. For VXI hardware triggers, VI_TRIG_PROT_DEFAULT is equivalent to VI_TRIG_PROT_SYNC. For PXI, VI_TRIG_PROT_RESERVE and VI_TRIG_PROT_UNRESERVE are the only valid protocols. |
Return Values
|
Type ViStatus |
This is the function return status. It returns either a completion code or an error code as follows. |
|
Completion Code |
Description |
|---|---|
|
VI_SUCCESS |
The specified trigger was successfully asserted to the device. |
|
Error Code |
Description |
|
VI_ERROR_BERR |
Bus error occurred during transfer. |
|
VI_ERROR_CONN_LOST |
The I/O connection for the given session has been lost. |
|
VI_ERROR_INP_PROT_VIOL |
Device reported an input protocol error occurred during transfer. |
|
VI_ERROR_INV_PROT |
The protocol specified is invalid. |
|
VI_ERROR_INV_SESSION |
The given session or object reference is invalid (both are the same value). |
|
VI_ERROR_INV_SETUP |
Unable to start operation because setup is invalid (due to attributes being set to an inconsistent state). |
|
VI_ERROR_LINE_IN_USE |
The specified trigger line is currently in use. |
|
VI_ERROR_NCIC |
The interface associated with the given vi is not currently the controller in charge. |
|
VI_ERROR_NLISTENERS |
No Listeners condition is detected (both NRFD and NDAC are deasserted). |
|
VI_ERROR_NSUP_OPER |
The given vi does not support this function. |
|
VI_ERROR_RAW_RD_PROT_VIOL |
Violation of raw read protocol occurred during transfer. |
|
VI_ERROR_RAW_WR_PROT_VIOL |
Violation of raw write protocol occurred during transfer. |
|
VI_ERROR_RSRC_LOCKED |
Specified operation could not be performed because the resource identified by vi has been locked for this kind of access. |
|
VI_ERROR_TMO |
Timeout expired before function completed. |
See Also
VI_ATTR_TRIG_ID
attribute. Set this attribute to the trigger mechanism/ trigger line to
use.
VI_EVENT_TRIG description
for details on trigger specifiers.