viEventHandler

Syntax

viEventHandler(ViSession vi, ViEventType eventType, ViEvent context, ViAddr userHandle);

Description

This is a prototype for a function, which you define. The function you define is called whenever a session receives an event and is enabled for handling events in the VI_HNDLR mode. The handler services the event and returns VI_SUCCESS on completion. VISA event handlers must be declared as follows.

ViStatus _VI_FUNCH MyEventHandler(ViSession vi, ViEventType eventType, ViEvent context, ViAddr userHandle);

The _VI_FUNCH declaration is required to make sure the handler is of the proper type. If _VI_FUNCH is not included, stack corruption may occur on the function call or return. The _VI_FUNCH declaration is very important since it declares the function of type stdcall that VISA requires. Visual Studio C++ defaults to cdecl that will not work. When the handler returns, it will generate an access violation because the stack gets corrupted.

Because each eventType defines its own context in terms of attributes, refer to the appropriate event definition to determine which attributes can be retrieved using the context parameter.

Because the event context must still be valid after the user handler returns (so that VISA can free it up), an application should not invoke the viClose operation on an event context passed to a user handler.

If the user handler will not return to VISA, the application should call viClose on the event context to manually delete the event object. This may occur when a handler throws a C++ exception in response to a VISA exception event.

Normally, an application should return VI_SUCCESS from all callback handlers. If a specific handler does not want other handlers to be invoked for the given event for the given session, it should return VI_SUCCESS_NCHAIN. No return value from a handler on one session will affect callbacks on other sessions.

This table lists events and associated read-only attributes implemented by Keysight VISA that can be read to get event information on a specific event. Use the viReadSTB function to read the status byte of the service request.

Please note, this function is available for both Windows and Linux users, however, VXI and PXI functionality are Windows only.

Instrument Control (INSTR) Resource Events

Event Name

Attributes

Data Type

Range

VI_EVENT_PXI_INTR

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_PXI_INTR

VI_EVENT_SERVICE_REQ

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_SERVICE_REQ

VI_EVENT_VXI_SIGP

VI_ATTR_EVENT_TYPE
VI_ATTR_SIGP_STATUS_ID

ViEventType
ViUInt16

VI_EVENT_VXI_STOP
0 to FFFFh

VI_EVENT_TRIG

VI_ATTR_EVENT_TYPE
VI_ATTR_RECV_TRIG_ID

ViEventType
ViInt16

VI_EVENT_TRIG
VI_TRIG_TTL0 to VI_TRIG_TTL11;
VI_TRIG_ECL0 to VI_TRIG_ECL5;
VI_TRIG_STAR_INSTR

VI_EVENT_IO_COMPLETION

VI_ATTR_EVENT_TYPE
VI_ATTR_STATUS
VI_ATTR_JOB_ID
VI_ATTR_BUFFER
VI_ATTR_RET_COUNT
VI_ATTR_RET_COUNT_32
VI_ATTR_RET_COUNT_64
VI_ATTR_OPER_NAME

ViEventType
ViStatus
ViJobId
ViBuf
ViUInt32
ViString

VI_EVENT_IO_COMPLETION
N/A
N/A
N/A
0 to FFFFFFFFh
N/A

VI_EVENT_VXI_VME_INTR

VI_ATTR_EVENT_TYPE
VI_ATTR_INTR_STATUS_ID
VI_ATTR_RECV_INTR_LEVEL

ViEventType
ViUInt32
ViInt16

VI_EVENT_VXI_VME_INTR
0 to FFFFFFFFh
1 to 7,  VI_UNKNOWN_LEVEL

Not supported by Keysight VISA:

   

VI_EVENT_USB_INTR

VI_ATTR_EVENT_TYPE
VI_ATTR_USB_RECV_INTR_SIZE
VI_ATTR_USB_RECV_INTR_DATA
VI_ATTR_STATUS

ViEventType
ViUInt16
ViBuf
ViStatus

VI_EVENT_USB_INTR
0 to FFFFh
N/A
N/A

Memory Access (MEMACC) Resource Events

Event Name

Attributes

Data Type

Range

VI_EVENT_IO_COMPLETION

VI_ATTR_EVENT_TYPE
VI_ATTR_STATUS
VI_ATTR_JOB_ID
VI_ATTR_BUFFER
VI_ATTR_RET_COUNT
VI_ATTR_RET_COUNT_32

VI_ATTR_RET_COUNT_64
VI_ATTR_OPER_NAME

ViEventType
ViStatus
ViJobId
ViBuf
ViUInt32
ViString

VI_EVENT_IO_COMPLETION
N/A
N/A
N/A
0 to FFFFFFFFh
N/A

GPIB Bus Interface (INTFC) Resource Events

Event Name

Attributes

Data Type

Range

VI_EVENT_GPIB_CIC

VI_ATTR_EVENT_TYPE
VI_ATTR_GPIB_RECV_CIC_STATE

ViEventType
ViBoolean

VI_EVENT_GPIB_CIC
VI_TRUE
VI_FALSE

VI_EVENT_GPIB_TALK

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_GPIB_TALK

VI_EVENT_GPIB_LISTEN

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_GPIB_LISTEN

VI_EVENT_CLEAR

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_CLEAR

VI_EVENT_TRIG

VI_ATTR_EVENT_TYPE
VI_ATTR_RECV_TRIG_ID

ViEventType
ViInt16

VI_EVENT_TRIG
VI_TRIG_SW

VI_EVENT_IO_COMPLETION

VI_ATTR_EVENT_TYPE
VI_ATTR_STATUS
VI_ATTR_JOB_ID
VI_ATTR_BUFFER
VI_ATTR_RET_COUNT
VI_ATTR_RET_COUNT_32

VI_ATTR_RET_COUNT_64
VI_ATTR_OPER_NAME

ViEventType
ViStatus
ViJobId
ViBuf
ViUInt32
ViString

VI_EVENT_IO_COMPLETION
N/A
N/A
N/A
0 to FFFFFFFFh
N/A

Backplane (BACKPLANE) Resource Events

Event Name

Attributes

Data Type

Range

VI_EVENT_TRIG

VI_ATTR_EVENT_TYPE
VI_ATTR_RECV_TRIG_ID

ViEventType
ViInt16

VI_EVENT_TRIG
VI_TRIG_TTL0 to VI_TRIG_TTL11;
VI_TRIG_ECL0 to VI_TRIG_ECL5;
VI_TRIG_STAR_SLOT1 to VI_TRIG_STAR_SLOT12

VI_EVENT_VXI_VME_SYSFAIL

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_VXI_VME_SYSFAIL

VI_EVENT_VXI_VME_SYSRESET

VI_ATTR_EVENT_TYPE

ViEventType

VI_EVENT_VXI_VME_SYSRESET

TCPIP Socket (SOCKET) Resource Events

Event Name

Attributes

Data Type

Range

VI_EVENT_IO_COMPLETION

VI_ATTR_EVENT_TYPE
VI_ATTR_STATUS
VI_ATTR_JOB_ID
VI_ATTR_BUFFER
VI_ATTR_RET_COUNT
VI_ATTR_RET_COUNT_32

VI_ATTR_RET_COUNT_64
VI_ATTR_OPER_NAME

ViEventType
ViStatus
ViJobId
ViBuf
ViUInt32
ViString

VI_EVENT_IO_COMPLETION
N/A
N/A
N/A
0 to FFFFFFFFh
N/A

Parameters

Name

Dir

Type

Description

vi

IN

ViSession

Unique logical identifier to a session.

eventType

IN

ViEventType

Logical event identifier.

context

IN

ViEvent

A handle specifying the unique occurrence of an event.

userHandle

IN

ViAddr

A value specified by an application that can be used for identifying handlers uniquely in a session for an event.

Return Values

Type ViStatus

This is the function return status. It returns either a completion code or an error code as follows.

Completion Code

Description

VI_SUCCESS

Event queue flushed successfully.

VI_SUCCESS_NCHAIN

Event handled successfully. Do not invoke any other handlers on this session for this event.

See Also

See Programming with VISA in the Keysight VISA User’s Guide for more information on event handling and exception handling.