viMapAddress
This section contains information specific to the Windows product.
Syntax
viMapAddress(ViSession vi, ViUInt16 mapSpace, ViBusAddress mapBase , ViBusSize mapSize, ViBoolean access, ViAddr suggested, ViPAddr address);
Description
This function maps in a specified memory space. The memory space that is mapped is dependent on the type of interface specified by the vi parameter and the mapSpace parameter (see the following table). The address parameter returns the address in your process space where memory is mapped. The values for the mapSpace parameter are:
|
Value |
Description |
|---|---|
|
VI_A16_SPACE |
Map the A16 address space of VXI/MXI bus. |
|
VI_A24_SPACE |
Map the A24 address space of VXI/MXI bus. |
|
VI_A32_SPACE |
Map the A32 address space of VXI/MXI bus. |
|
VI_A64_SPACE |
Address the A64 address space of VXI/MXI bus. |
|
VI_PXI_CFG_SPACE |
Address the PCI configuration space. |
|
VI_PXI_BAR0_SPACE – VI_PXI_BAR5_SPACE |
Address the specified PCI memory or I/O space. |
|
VI_PXI_ALLOC_SPACE |
Access physical locally allocated memory. |
- If the viSession parameter (vi) refers to an INSTR session, the mapBase parameter specifies a relative offset in the instrument’s mapSpace. If the ViSession parameter (vi) refers to a MEMACC session, the mapBase parameter is an absolute offset from the start of the VXI mapSpace.
|
For a given session, you can only have one map at one time. If you need to have multiple maps to a device, you must open one session for each map needed. |
- The mapBase parameter specified
in the viMapAddress operation
for an INSTR resource is the offset address relative to the device's allocated
address base for the corresponding address space specified. For example, if mapSpace specifies
VI_A16_SPACE, mapBase specifies
the offset from the logical address base address of the VXI device specified.
If mapSpace specifies VI_A24_SPACE, VI_A32_SPACE,
or VI_A64_SPACE, mapBase specifies
the offset from the base address of the VXI device's memory space allocated
by the VXI Resource Manager within VXI A24, A32, or A64 space.
- When calling the viMapAddress function on a PXI session, the maximum value for the mapSize parameter is limited to the actual size of the resource addressed by the mapSpace parameter (VI_PXI_BAR0_SPACE – VI_PXI_BAR5_SPACE).
|
viMapAddress is not supported for use with VBA on 64-bit systems. |
Parameters
|
Name |
Dir |
Type |
Description |
|---|---|---|---|
|
vi |
IN |
ViSession |
Unique logical identifier to a session. |
|
mapSpace |
IN |
ViUInt16 |
Specifies the address space to map. |
|
mapBase |
IN |
ViBusAddress |
Offset (in bytes) of the memory to be mapped. |
|
mapSize |
IN |
ViBusSize |
Amount of memory to map (in bytes). |
|
access |
IN |
ViBoolean |
VI_FALSE. |
|
suggested |
IN |
ViAddr |
If suggested parameter is not VI_NULL, the operating system attempts to map the memory to the address specified in suggested. There is no guarantee, however, that the memory will be mapped to that address. This function may map the memory into an address region different from suggested. |
|
address |
OUT |
ViPAddr |
Address in your process space where the memory was mapped. |
Return Values
|
Type ViStatus |
This is the function return status. It returns either a completion code or an error code as follows. |
|
Completion Code |
Description |
|---|---|
|
VI_SUCCESS |
Map successful. |
|
Error Code |
Description |
|
VI_ERROR_ALLOC |
Unable to allocate window of at least the requested size. |
|
VI_ERROR_INV_ACC_MODE |
Invalid access mode. |
|
VI_ERROR_INV_OFFSET |
Invalid offset specified. |
|
VI_ERROR_INV_SESSION |
The given session or object reference is invalid (both are the same value). |
|
VI_ERROR_INV_SETUP |
Unable to start operation because the setup is invalid (due to attributes being set to an inconsistent state). |
|
VI_ERROR_INV_SIZE |
Invalid size of window specified. |
|
VI_ERROR_INV_SPACE |
Invalid mapSpace specified. |
|
VI_ERROR_NSUP_OFFSET |
Specified region is not accessible from this hardware. |
|
VI_ERROR_NSUP_OPER |
The given vi does not support this operation. |
|
VI_ERROR_RSRC_LOCKED |
Specified operation could not be performed because the resource identified by vi has been locked for this kind of access. |
|
VI_ERROR_TMO |
viMapAddress could not acquire resource or perform mapping before the timer expired. |
|
VI_ERROR_WINDOW_MAPPED |
The specified session already contains a mapped window. |