viOpenDefaultRM
Syntax
viOpenDefaultRM(ViPSession sesn);
Description
This function returns a session to the Default Resource Manager resource. This function must be called before any VISA functions can be invoked. The first call to this function initializes the VISA system, including the Default Resource Manager resource, and also returns a session to that resource. Subsequent calls to this function return unique sessions to the same Default Resource Manager resource.
Parameters
| 
                                                     Name  | 
                                                
                                                     Dir  | 
                                                
                                                     Type  | 
                                                
                                                     Description  | 
                                            
|---|---|---|---|
| 
                                                     sesn  | 
                                                
                                                     OUT  | 
                                                
                                                     ViPSession  | 
                                                
                                                     Unique logical identifier to a Default Resource Manager session.  | 
                                            
Return Values
| 
                                                     Type ViStatus  | 
                                                
                                                     This is the function return status. It returns either a completion code or an error code as follows.  | 
                                            
| 
                                                     Completion Code  | 
                                                
                                                     Description  | 
                                            
|---|---|
| 
                                                     VI_SUCCESS  | 
                                                
                                                     Session to the Default Resource Manager resource created successfully.  | 
                                            
| 
                                                     Error Code  | 
                                                
                                                     Description  | 
                                            
| 
                                                     VI_ERROR_ALLOC  | 
                                                
                                                     Insufficient system resources to create a session to the Default Resource Manager resource.  | 
                                            
| 
                                                     VI_ERROR_INV_SETUP  | 
                                                
                                                     Some implementation-specific configuration file is corrupt or does not exist.  | 
                                            
| 
                                                     VI_ERROR_SYSTEM_ERROR  | 
                                                
                                                     The VISA system failed to initialize.  | 
                                            
C# Example
public int OpenRM() { int resourceManager, viError; viError = visa32.viOpenDefaultRM(out resourceManager); if (viError < visa32.VI_SUCCESS) throw new ApplicationException( "Failed to open Resource Manager"); return resourceManager; }
VB .NET Example
Public Function OpenRM() As Integer Dim resourceManager As Integer = 0, viError As Integer viError = visa32.viOpenDefaultRM(resourceManager) If viError < visa32.VI_SUCCESS Then Throw New ApplicationException("Failed to open Resource Manager") End If Return resourceManager End Function