viVScanf
Syntax
viVScanf(ViSession vi, ViString readFmt, ViVAList params);
Description
This function reads, converts, and formats data using the format specifier and then stores the formatted data in params. This function is similar to viScanf, except that the ViVAList parameters list provides the parameters rather than separate arg parameters.
Using viVScanf in Visual Basic 6
                                            
 This section contains information specific to the Windows product.
The viPrintf, viScanf, and viQueryf VISA functions take variable argument lists in C. Some of viScanf's and viQueryf's variable arguments are references to primitive (byte, integer, long, float, etc.) types, meaning that the values themselves can be changed by the function. There is no equivalent in VB6 for variable argument lists with reference arguments, so no direct translation is available. Instead, use the 'V' form of these functions (viVPrintf, viVScanf, and viVQueryf), in conjunction with the undocumented VB6 VarPtr function to create an array of pointers to arguments than can be passed to the VISA functions.
The examples below are presented as self-contained VB6 Sub's with comments explaining the various features. You can modify and adapt the code in the examples to your specific situation.
Parameters
                                            
                                            
This section contains information that applies to both Windows and Linux.
| 
                                                     Name  | 
                                                
                                                     Dir  | 
                                                
                                                     Type  | 
                                                
                                                     Description  | 
                                            
|---|---|---|---|
| 
                                                     vi  | 
                                                
                                                     IN  | 
                                                
                                                     ViSession  | 
                                                
                                                     Unique logical identifier to a session.  | 
                                            
| 
                                                     readFmt  | 
                                                
                                                     IN  | 
                                                
                                                     ViString  | 
                                                
                                                     The format string to apply to parameters in ViVAList. See viScanf for description.  | 
                                            
| 
                                                     params  | 
                                                
                                                     OUT  | 
                                                
                                                     ViVAList  | 
                                                
                                                     A list with the variable number of parameters into which the data is read and the format string is applied.  | 
                                            
Return Values
| 
                                                     Type ViStatus  | 
                                                
                                                     This is the function return status. It returns either a completion code or an error code as follows.  | 
                                            
| 
                                                     Completion Code  | 
                                                
                                                     Description  | 
                                            
|---|---|
| 
                                                     VI_SUCCESS  | 
                                                
                                                     Data were successfully read and formatted into arg parameter(s).  | 
                                            
| 
                                                     Error Code  | 
                                                
                                                     Description  | 
                                            
| 
                                                     VI_ERROR_ALLOC  | 
                                                
                                                     The system could not allocate a formatted I/O buffer because of insufficient resources.  | 
                                            
| 
                                                     VI_ERROR_INV_FMT  | 
                                                
                                                     A format specifier in the readFmt string is invalid.  | 
                                            
| 
                                                     VI_ERROR_INV_SESSION  | 
                                                
                                                     The given session or object reference is invalid (both are the same value).  | 
                                            
| 
                                                     VI_ERROR_IO  | 
                                                
                                                     Could not perform read function because of I/O error.  | 
                                            
| 
                                                     VI_ERROR_NSUP_FMT  | 
                                                
                                                     A format specifier in the readFmt string is not supported.  | 
                                            
| 
                                                     VI_ERROR_RSRC_LOCKED  | 
                                                
                                                     Specified operation could not be performed because the resource identified by vi has been locked for this kind of access.  | 
                                            
| 
                                                     VI_ERROR_TMO  | 
                                                
                                                     Timeout expired before read function completed.  | 
                                            
See Also
viScanf 
viVPrintf/viVScanf Example using String
viVScanf Example Returning a Double Array
viVScanf Example Reading an IEEE 488 Definite Length Block and Returning 
 a Byte Array
viVScanf Example Reading an IEEE 488 Indefinite Length Block and Returning 
 a Byte Array