viWaitOnEvent
This section contains information that applies to both Windows and Linux.
Specific items that apply in Windows only will be marked with a
icon.
Syntax
viWaitOnEvent(ViSession vi, ViEventType inEventType, ViUInt32 timeout, ViPEventType outEventType, ViPEvent outContext);
Description
This function waits for an occurrence of the specified event for a given session. In particular, this function suspends execution of an application thread and waits for an event inEventType for at least the time period specified by timeout. See the individual event descriptions for context definitions.
If the specified inEventType is VI_ALL_ENABLED_EVENTS, the function waits for any event that is enabled for the given session. If the specified timeout value is VI_TMO_INFINITE, the function is suspended indefinitely to wait for an occurrence of an event.
If the value VI_TMO_IMMEDIATE is specified in the timeout parameter of viWaitOnEvent, application execution is not suspended. This operation can be used to dequeue events from an event queue by setting the timeout value to VI_TMO_IMMEDIATE.
viWaitOnEvent removes the specified event from the event queue if one that matches the type is available. The process of dequeuing makes an additional space available in the queue for events of the same type.
You must call viEnableEvent to enable the reception of events of the specified type before calling viWaitOnEvent. viWaitOnEvent does not perform any enabling or disabling of event reception.
If the value VI_NULL is specified in the outContext parameter of viWaitOnEvent and the return value is successful, viClose is automatically invoked on the event context rather than returning it to the application. Important: C/C++ programs do this, see Note on Context Return in visa32.cs and visa32.vb below.
The outEventType and outContext parameters to the viWaitOnEvent operation are optional. They can be used if the event type is known from the inEventType parameter or if the eventContext is not needed to retrieve additional information.
|
Since system resources are used when waiting for events (viWaitOnEvent), the viClose function must be called to free up event contexts (outContext). |
This table lists events and associated read-only attributes implemented by Keysight VISA that can be read to get event information on a specific event. Use the viReadSTB function to read the status byte of the service request.
Instrument Control (INSTR) Resource Events
|
Event Name |
Attributes |
Data Type |
Range |
|---|---|---|---|
|
VI_EVENT_SERVICE_REQ |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_SERVICE_REQ |
|
VI_EVENT_VXI_SIGP |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_VXI_STOP |
|
VI_EVENT_TRIG |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_TRIG |
|
VI_EVENT_IO_COMPLETION |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_IO_COMPLETION |
|
VI_EVENT_VXI_VME_INTR |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_VXI_VME_INTR |
|
VI_EVENT_PXI_INTR |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_PXI_INTR |
|
VI_EVENT_USB_INTR |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_USB_INTR |
Memory Access (MEMACC) Resource Events
This section contains information specific to the Windows product.
|
Event Name |
Attributes |
Data Type |
Range |
|---|---|---|---|
|
VI_EVENT_IO_COMPLETION |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_IO_COMPLETION |
GPIB Bus Interface (INTFC) Resource Events
|
Event Name |
Attributes |
Data Type |
Range |
|---|---|---|---|
|
VI_EVENT_GPIB_CIC |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_GPIB_CIC |
|
VI_EVENT_GPIB_TALK |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_GPIB_TALK |
|
VI_EVENT_GPIB_LISTEN |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_GPIB_LISTEN |
|
VI_EVENT_CLEAR |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_CLEAR |
|
VI_EVENT_TRIG |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_TRIG |
|
VI_EVENT_IO_COMPLETION |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_IO_COMPLETION |
Backplane (BACKPLANE) Resource Events
This section contains information specific to the Windows product.
|
Event Name |
Attributes |
Data Type |
Range |
|---|---|---|---|
|
VI_EVENT_TRIG |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_TRIG |
|
VI_EVENT_VXI_VME_SYSFAIL |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_VXI_VME_SYSFAIL |
|
VI_EVENT_VXI_VME_SYSRESET |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_VXI_VME_SYSRESET |
TCPIP Socket (SOCKET) Resource
|
Event Name |
Attributes |
Data Type |
Range |
|---|---|---|---|
|
VI_EVENT_IO_COMPLETION |
VI_ATTR_EVENT_TYPE |
ViEventType |
VI_EVENT_IO_COMPLETION |
Parameters
|
Name |
Dir |
Type |
Description |
|---|---|---|---|
|
vi |
IN |
ViSession |
Unique logical identifier to a session. |
|
inEventType |
IN |
ViEventType |
Logical identifier of the event(s) to wait for. |
|
timeout |
IN |
ViUInt32 |
Absolute time period in time units that the resource shall wait for a specified event to occur before returning the time elapsed error. The time unit is in milliseconds. |
|
outEventType |
OUT |
ViPEventType |
Logical identifier of the event actually received. |
|
outContext |
OUT |
ViPEvent |
A handle specifying the unique occurrence of an event. |
Special Values for outEventType Parameter |
|||
|
Value |
Description |
||
|
VI_NULL |
|
|
Do not return the type of event. |
Special Value for outContext Parameter |
|||
|
Value |
Description |
||
|
VI_NULL |
|
|
Do not return an event context. |
Return Values
|
Type ViStatus |
This is the function return status. It returns either a completion code or an error code as follows. |
|
Completion Code |
Description |
|---|---|
|
VI_SUCCESS |
Wait terminated successfully on receipt of an event occurrence. The queue is empty. |
|
VI_SUCCESS_QUEUE_NEMPTY |
Wait terminated successfully on receipt of an event notification. There is still at least one more event occurrence of the specified inEventType type available for this session. |
|
Error Code |
Description |
|
VI_ERROR_INV_EVENT |
Specified event type is not supported by the resource. |
|
VI_ERROR_INV_SESSION |
The given session or object reference is invalid (both are the same value). |
|
VI_ERROR_TMO |
Specified event did not occur within the specified time period. |
Note on Context Return in visa32.cs and visa32.vb
This section contains information specific to the Windows product.
It is not possible to pass a 'null' pointer for the 'ref context' parameter in viWaitOnEvent as it is defined in visa32.cs and visa32.vb. This means that VISA will not close the context and when viWaitOnEvent is called in a loop, the system will eventually run out of resources.
The solution is to close the returned context after a successful return from viWaitOnEvent. Here is some C# sample code that works:
...
int context = 0;
err = visa32.viWaitOnEvent(vi, visa32.VI_EVENT_SERVICE_REQ, 500, ref eventType, ref context);
if (err >= visa32.VI_SUCCESS)
{
visa32.viClose(context);
}
...
See Also
See Programming with VISA for more information on event handling.