The adjustment determines the power detected by the A8 Analog IF (AIF) input power detector under known conditions. The detector gives a DC level which corresponds to this power. An ADC converts this DC level to a digital value which is then stored in the A8 EEPROM.
The 321.4 MHz calibrator on the A10 Third Converter is used to provide a stable -7 dBm, 21.4 MHz signal to the A8 input. A power meter is used to measure this signal at A10J5 to accurately set its power level.
This adjustment should be performed after replacing the A8 assembly.
|
|
This adjustment saves an output file which lists the corrections that were stored in the instrument. The output file is saved at this location:
|
|
Test Equipment |
Model Number |
|---|---|
|
Power Meter |
N1914B |
|
Power Sensor |
N8481A |
|
Type-N (f) to BNC (m) adapter |
1250-1477 |
|
SMB (f) to BNC (f) adapter |
1250-1236 |