In this test, the power bandwidth function is checked at a CW frequency of 50 MHz for resolution bandwidths from 3 Hz to 1 MHz in a 1, 3, 10 sequence. The signal source is the internal 50 MHz calibrator signal. The power bandwidth function reads the integrated power between a marker pair which enclose the CW signal.. This power is compared to the maximum power of the CW signal as read by the E444XA marker.
Click here for troubleshooting.
None