This test determines that the frequency reference is functional, provides a measured frequency value, suggests that an adjustment be made if the yearly allowable frequency offset value is exceeded.
The instrument is set to Internal Reference mode and is allowed a sufficient warm-up time of 30 minutes while powered on (not in Standby mode). The frequency of the 10 MHz Reference is measured at its rear-panel port using a counter locked to a frequency standard. The measured value is compared to the allowable offset guideline, and is also printed on the Performance Test printout.
Placing the analyzer in Standby mode turns the frequency reference oscillator off, while continuing to provide power to the oven. While keeping the oscillator warm will reduce its stabilization time, it will not cause aging.
Click here for troubleshooting.
|
Test Equipment |
Model Number |
|---|---|
|
Universal Counter |
53230A |
|
Frequency Standard1 |
Microsemi 5071A-C002 |
|
BNC Cable (2 required) |
8120-2582 |
|