Resolution bandwidth switching uncertainty is the relative amplitude error caused by the multiple filters that produce a specific RBW. To measure the resolution bandwidth switching uncertainty, an amplitude reference is taken with the resolution bandwidth set to 30 kHz using the marker delta function The resolution bandwidth is changed to settings between 300 Hz and 8 MHz, as applicable, and the relative amplitude variation is measured at each setting and compared to the specification.
Click here for troubleshooting.
None