The PSA Resolution Bandwidth Filters are implemented through DSP. The A8 Analog IF contains discrete IF Prefilters. The prefilters prevent unwanted images from entering the ADC. These prefilters are set much wider than the RBW setting to prevent any interference with the Bandwidth shape factor. If the prefilters have become defective, they may affect the RBW shape factor.