This section lists the test equipment needed to run performance tests. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. All equipment is Keysight, Agilent, or Hewlett Packard unless otherwise specified. Refer to each individual test for specific setup configurations.
|
|
UXA models with frequency option 526 will be tested on the 2.4 mm connector — not the 2.4 mm to 3.5 mm adapter. Remove the adapter if it's present on the DUT. |
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Sources |
||
|
Signal generator
|
E8257D with options:
|
E8267D with options:
(1E1 and 1EU are standard options) |
|
Ultra low-noise reference frequency source |
Wenzel 500-13438 Rev D |
Wenzel 500-13438 Rev C |
|
Analyzers |
||
|
Network analyzer |
PNA N5247B Option 425
|
PNA N5245B Option 425
|
|
Meters |
||
|
Power meter |
N1914A1, 2 |
|
|
Digital multimeter |
3458A |
|
|
Power Sensors (See below for calibration service ordering guidelines.) |
||
|
Millimeter power sensor, 2.4 mm, 50 GHz
|
N8487A |
U8487A2 |
|
Millimeter power sensor, 2.4 mm, 50 GHz |
U8487A2 |
None |
|
Low-power power sensor, 2.4 mm, 50 GHz
|
8487D |
|
|
Power sensor, Type-N, 9 kHz to 6 GHz
|
E9304A |
|
|
Power sensor, Type-N, 100 kHz to 6 GHz
|
N8482A |
|
|
Power sensor, 3.5 mm, 26.5 GHz
|
N8485A |
U8485A |
|
Attenuators |
||
|
6 dB attenuator, fixed, Type-N |
8491A Option 006, H33 |
8491B Option 006, H33 |
|
6 dB attenuator, fixed, 2.4 mm
|
8490D Option 006 |
|
|
10 dB attenuator, fixed, Type-N |
8491A Option 010, H33 |
8491B Option 010, H33 |
|
6 dB attenuator, fixed, 3.5 mm
|
8493C Option 006 |
|
|
30 dB attenuator, fixed
|
11708A |
|
|
1 dB step attenuator3 |
8494G Option 001, H50 |
8494H Option 001, H50 |
|
10 dB step attenuator3 |
8496G Option 001, H50 |
8496H Option 001, H50 |
|
Filters |
||
|
Band pass filter, 1 GHz |
0955-1612 |
|
|
Low pass filter, 5 GHz, SMA (f) to SMA (f) |
RLC F-30-5000-RF |
|
|
Low pass filter, 50 MHz
|
Mini-Circuits NLP-50+ |
|
|
Low pass filter, 190 MHz
|
Mini-Circuits VLF190+ |
|
|
Low pass filter, 530 MHz
|
Mini-Circuits VLF-530+ |
|
|
Low pass filter, 1575 MHz
|
Mini-Circuits VLFG-1575+ |
|
|
Low pass filter, 3900 MHz
|
Mini-Circuits VLF-3800+ |
|
|
Low pass filter, 11000 MHz
|
Mini-Circuits ZLFW-K113+ |
|
|
Low pass filter, 21000 MHz
|
Mini-Circuits ZLSS-K21G+ |
|
|
Miscellaneous devices |
||
|
Frequency counter |
53230A |
|
|
Frequency standard |
Microsemi 5071A |
10 MHz external reference (house standard) |
|
Power splitter, 2.4 mm, 50 GHz
|
11667C |
|
|
Power splitter, Type-N, 18 GHz |
11667A |
|
|
ECal, 2.4 mm, 50 GHz |
N4693D Option M0F |
|
|
Load, 2.4 mm (f), 50 Ω |
85138B |
|
|
Attenuator driver |
11713D |
11713E |
|
Attenuator interconnect kit
|
11716A |
|
|
50 Ω feedthrough, BNC (m) to BNC (f)
|
0960-0301 |
11048C |
|
Cables |
||
|
Cable, BNC |
8120-1840 |
8120-2582 |
|
Cable, 2.4 mm (f) to 2.4 mm (m)
|
8121-2065 (or equivalent) |
8120-6192 |
|
Adapters |
||
|
Banana plug, dual, BNC (f) |
1251-2277 |
|
|
|||||||||||||||||||||||||||||||||||||||||
Use the following guidelines to ensure power sensors used by the N78000B application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N78000B ETMS calibrations.
When ordering periodic calibration for instruments used as lab standards in the N78000B software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N78000B software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N78000B measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N78000B calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into ETMS thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|