|
|
This test applies only to analyzers that are not equipped with the high stability frequency reference, Option 1D5. If your analyzer has Option 1D5, perform 10 MHz High Stability Frequency Reference Accuracy, (Opt 1D5) instead. |
The settability is measured by changing the setting of the digital-to-analog converter (DAC) which controls the frequency of the timebase. The frequency difference per DAC step is calculated and compared to the specification.
|
Related specification: |
Frequency Reference: Settability |
|
Related adjustment: |
|
Equipment |
Recommended Model |
For ESA Models |
|
Frequency Counter 1 |
53230A |
All |
|
Frequency Standard 1 |
Microsemi 5071A-C002 |
All |
|
Cable, BNC, 2 required |
8120-2582 |
All |
The 10 MHz reference settability is calculated using the following equation:
|