IF Flatness Adjustment

This adjustment characterizes the flatness of the IF filter response. Any “unflatness” of the IF filter response can manifest itself as additional frequency response error or resolution bandwidth switching uncertainty.

To measure IF Flatness, the analyzer’s center frequency and DDC frequency are set such that the IF flatness over a 2 MHz bandwidth can be measured. This process is repeated at 12 different analyzer center frequencies, thus characterizing the IF over a 24 MHz total bandwidth. These measurements are made once in low band, at a nominal center frequency of less than 2.7 GHz, and again in high band, at a nominal center frequency of greater than 2.7 GHz.

The measured data is normalized to the measurements at the last IF’s nominal center frequency of 45 MHz. The data is then stored in the analyzer’s non-volatile memory.

Related Specifications


Required Test Equipment 

Test Equipment

Model Number

Synthesized Signal Generator

E8267D

Frequency Standard

5071A

Power Meter

E4419B

Power Sensor

E9304A

Power Splitter

11667A

Attenuator, 1 dB Step

8494H

Attenuator, 10 dB Step

8496H

Attenuator/Switch Driver

11713A

Cable, Type-N (2 required)

11500C

Cable, BNC (2 required)

10503A

Adapter, Type-N (m) to Type-N (m)

1250-1475

Attenuator, 6 dB Fixed

8491A Option 006

Connection Setups