CXA — N9000A/B
The adjustment generates the tracking generator amplitude corrections which are stored in memory. This adjustment should only be performed if the tracking generator has been replaced, or if it fails the Absolute Amplitude and Flatness test.
Click here for troubleshooting.
|
Test Equipment |
Recommended Model Number |
|---|---|
|
Signal Analyzer |
N9030B |
|
Power Meter |
N1914B |
|
RF Power Sensor |
E9304A Option H18 |
|
Type-N Cable |
11500C |
|
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |