Freq Resp AC Coupled Adjustment

This adjustment applies to the following models:

This adjustment determines the frequency at which the AC Coupling capacitor attenuates the input signal 3 dB. This frequency is stored in memory and the analyzer applies the appropriate correction for the capacitor rolloff.

Click here for troubleshooting.

Required Test Equipment

Test Equipment

Recommended Model Number

Function Generator

33622A 

BNC Cable
(2 required)

8120-1840 

Type-N (m) to BNC (f) adapter

1250-1476

Connection Setups

In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines.

Frequency Response (AC Coupled) Adjustment Setup