Backup Cal Data to Instrument Memory

This procedure applies to the following models:

This utility is run after running adjustments to save calibration data to the DUT. The data will be saved to either secure memory, an SD card, or SSD drive, or any combination if they are present.

Although the Backup Cal Data to Instrument Memory is a utility, it can also be run from the Adjustments Test Plan for convenience.